Symbol: 
Function: This command adds the variable of the current location of the cursor to a watchlist for the purpose of online monitoring.
Call: Right-click a variable in an editor when the application is in online mode.
This command adds the variable to the currently opened watchlist. If a watchlist is not open, then the variable is added to the “Watch 1” list and that view opens.