Symbol: 
 
Function: This command opens the “Breakpoints” view.
Call: Menu bar: “View”.
This view shows an overview of all defined breakpoints for an application. You have access to all breakpoint commands within this view.
| 
                                  “Application”  | 
                              
                                  Select the required application from the list.  | 
                           
| 
                                  “POU”  | 
                              
                                  Name of the function block that will receive the breakpoint  | 
                           
| 
                                  “Location”  | 
                              
                                  Location of the breakpoint in the POU 
 For function blocks, "(Impl)" indicates that the breakpoint is located in the implementation of the function block, not in an instance.  | 
                           
| 
                                  “Instance Path”  | 
                              
                                  Complete object path of the breakpoint location.  | 
                           
| 
                                  “Tasks”  | 
                              
                                  Names of tasks that will be effective when the breakpoint is executed. If there are no restrictions, then "(all)" is displayed here.  | 
                           
| 
                                  “Condition”  | 
                              
                                 
  | 
                           
| 
                                  “Hit Count Condition”  | 
                              
                                  When the breakpoint should be in effect (depending on the hit count)  | 
                           
| 
                                  “Current Hit Count”  | 
                              
                                  How often the breakpoint has already been reached up to now during the execution  | 
                           
![]()  | 
                              
                                  
  | 
                              
                                  This command opens the “Breakpoint Properties” dialog.  | 
                           
| 
                                  
  | 
                              
                                  This command opens the “New Breakpoint” dialog.  | 
                           |
![]()  | 
                              
                                  “Clear Breakpoint”  | 
                              
                                  Removes the breakpoint (not the same as disable)  | 
                           
![]()  | 
                              
                                  “Enable/Disable Breakpoint”  | 
                              
                                  Toggles the status of the breakpoint or execution point between "enabled" and "disabled" 
 As opposed to "Clear breakpoint", a disabled breakpoint remains in the list and can be enabled again.  | 
                           
![]()  | 
                              
                                  “Properties”  | 
                              
                                  The “Breakpoint Properties” dialog opens for editing the breakpoint parameters. This dialog is the same as “New Breakpoint”. In online mode, you can change the breakpoint into an execution point.  | 
                           
![]()  | 
                              
                                  “Go to Source Position”  | 
                              
                                  Opens the online view of the affected block. The cursor is set at the breakpoint location.  | 
                           
![]()  | 
                              
                                  “Clear All Breakpoints”  | 
                              
                                  Deletes all breakpoints and execution points in the application. The list is cleared. Not to be confused with "deactivate".  | 
                           
![]()  | 
                              
                                  “Enable All Breakpoints”  | 
                              
                                  Enables all currently disabled breakpoints and execution points.  | 
                           
![]()  | 
                              
                                  “Disable All Breakpoints”  | 
                              
                                  Disables all currently enabled breakpoints and execution points. The points remain in the list and can be enabled again.  | 
                           





 Breakpoint disabled
 Execution point enabled
 Execution point disabled
 Data breakpoint disabled
 Data execution point enabled
 Data execution point disabled