Symbol: 
Function: This command checks whether the ID of a text list entry in the project is correct and reports the result.
Call: Main menu “Textlist”, context menu
Requirement: The “GlobalTextList” is open and active. A field in the table is selected.
If CODESYS finds during checking that the global text list and the static texts of the visualizations do not correspond, this could be because the global text list is or was write protected. The requirement for this is that you have set up a user management system in the project.
See also