Function: The command opens the dialog “Edit Declaration Header”, which serves in the declaration editor for the configuration of a POU header.
Call: Context menu of the tabular declaration editor
Requirements: The tabular declaration editor is the active editor.
Dialog 'Edit Declaration Header'
Function: The dialog is for configuring the declaration part of a POU.
Call: Click on the header bar of the tabular declaration editor, or context menu in the tabular declaration editor.
| 
                                  “Declaration”  | 
                              
                                  Selection list for changing the POU type 
 Input field with current POU name: you can change the name of the POU  | 
                           
| 
                                  “Automatically adapt all references on rename”  | 
                              
                                  
 
  | 
                           
| 
                                  “Attributes”  | 
                              
                                  The dialog box “Attribute ” opens for the input of attributes and pragmas.  | 
                           
: Dialog box 
: Renaming is only effective in the declaration header of the POU.