Symbol: 
Function: The command starts an automatic formatting of the code in the open ST editor.
Call: Menu bar: “Edit Advanced”; context menu of the window in focus in the ST editor
Requirement: The focus is in the ST editor. The syntax of the ST code does not contain any errors.
The following formatting is performed automatically:
- 
                           
Keywords are converted to uppercase letters.
 - 
                           
Spacing is standardized.
 - 
                           
Indentations are changed according to syntax.
 - 
                           
Long lines are wrapped in sensible places.
 
See also