Symbol
; shortcut: [F11]
Function: The command starts the code generation for the active application.
Call: Menu bar: “Build”
When generating code with this command, code is generated as when downloading the application to the PLC, but the code is not transferred to the PLC. At this time, other source code tests are performed As a result, you can check the code for bugs that were not detected by the compiler and for fixing any bugs before the code is used in online mode.
See also