Symbol: 
Function: The command opens the declaration location of the variable that is referenced by the pointer currently in focus in online mode.
Call:
- 
                           
Context menu in the declaration part or implementation code
 - 
                           
Menu bar: “Edit Browse”
 
Requirement: Online mode. A POU is open in the editor and the cursor is at a pointer. The referenced variable is stored in static memory.
If the pointer does not point exactly to the beginning of the variable, then a corresponding message is displayed when you switch to the variable declaration.
See also