Symbol: 
Function: The command opens the “Library Repository” dialog. In this dialog you define which libraries are installed on the local system and are thus available for your application.
Call: Menu bar: “Tools”
Dialog 'Library Repository'
| 
                                  Display of the directory on the local system in which the library files are located. The libraries in this “Location” are listed in the “Installed libraries” area.  | 
                           |
| 
                                  “Edit Locations”  | 
                              
                                  Opens the “Edit Repository Locations” dialog.  | 
                           
1. You can only use empty directories for new repositories.
2. You can also use existing repositories as locations.
3. The "System" repository is not editable; CODESYS indicates this by the italic lettering of the entry.
| 
                                  List of the repositories with “Location” and “Name”  | 
                           |
| 
                                  “Add”  | 
                              
                                  Creates a new repository. Opens the “Repository Location” dialog. The selected directory (“Location” input field) has to be either empty or an existing valid repository. “Name” is the input field for a symbolic repository name.  | 
                           
| 
                                  “Edit”  | 
                              
                                  Opens the “Repository Location” dialog (see “Add”)  | 
                           
| 
                                  “Remove ”  | 
                              
                                  A dialog box open, asking whether only the entry should be removed from the list of repositories, or whether the directory with the library files should be deleted from the file system. If you want to delete the directory, you have to confirm this.  | 
                           
| 
                                  List of the libraries in a tree structure. Display of each library with category,
                                    name, company and version. The icon to the left of the name indicates whether the
                                    library is   | 
                           |
| 
                                  “Company ”  | 
                              
                                  List box for filtering the displayed libraries.  | 
                           
| 
                                  “Install”  | 
                              
                                  Opens the “Select Library” dialog. Possible filters: 
  | 
                           
| 
                                  “Uninstall”  | 
                              
                                  Uninstalls the selected library.  | 
                           
| 
                                  “Export”  | 
                              
                                  Opens the default dialog for saving the library project to the local file system.
                                    The file type is   | 
                           
| 
                                  “Find”  | 
                              
                                  Searches for libraries and function blocks. Opens the “Find Library” dialog. When you enter a string in the input field, CODESYS displays the libraries that it finds with a corresponding string.  | 
                           
| 
                                  “Details”  | 
                              
                                  Opens the “Details” dialog with details from the project information of the library for the selected version of a library. You find the following information by clicking “More” in the “Details” dialog: 
  | 
                           
| 
                                  “Dependencies”  | 
                              
                                  For the selected library, the “Dependencies” dialog opens, showing the dependencies on other libraries. “Title”, “Version” and “Company” are shown for each library reference. References that function via placeholders are displayed according to the syntax: #<placeholder name>.  | 
                           
| 
                                  “Group by category”  | 
                              
                                 
 The categories are defined by external description files '*.libcat.xml'.  | 
                           
| 
                                  A library profile defines the library version with which CODESYS resolves a library placeholder if a certain compiler version is set in the project.  | 
                           |
| 
                                  “Import”  | 
                              
                                  Imports a  If the import already contains existing placeholder entries, a query appears asking whether CODESYS should overwrite it.  | 
                           
| 
                                  “Export”  | 
                              
                                  Exports an xml file with the extension   | 
                           
Placeholder resolutions can also be defined in the target device currently in use and even by a specific local specification in the Placeholders dialog in the Library Manager.
 digitally signed or 
 unsigned. 
: Grouping by library category 
: Alphabetical sorting