Symbol: 
; shortcut: [Ctrl]+[O] 
Function: The command opens the default dialog for loading a project. You can search for a CODESYS project in the file system and open it in the development system.
Call: Menu bar: “File”
Dialog 'Open Project'
| 
                                  “File type”  | 
                              
                                  Type of the CODESYS project to be loaded to the development system  | 
                           
| 
                                  “All supported files”  | 
                              
                                  Filters by all projects which CODESYS can load Hint: For example, you can select   | 
                           
| 
                                  File extension   | 
                              
                                  Filters by projects which have been created with CODESYS V3  | 
                           
| 
                                  File extension   | 
                              
                                  Filters by project archives which have been created with CODESYS V3  | 
                           
| 
                                  File extension   | 
                              
                                  Filters by library projects which have been created with CODESYS V3  | 
                           
| 
                                  “Open”  | 
                              
                                  Loads the project you selected to CODESYS Note: Depending on the state of your CODESYS installation, it may be necessary to update or supplement the installation. If this is the case, then first open another “Open Project” dialog with options for installation management.  |