Function: This command opens the “Placeholders” dialog box. The dialog shows information on the currently selected placeholder library and allows to assign a project-specific resolution.
Call:
- 
                           
Menu “Libraries”
 - 
                           
Symbol
 in the symbol bar in the upper part of the Library Manager window. 
Requirement: A placeholder library is selected in the Library Manager.
A placeholder library, which is included in the “Devices” view, will be resolved as follows:
- 
                           
If you have assigned a specific resolution to the placeholder library via the dialog “Placeholder”, this will be applied.
 - 
                           
If no specific resolution is defined, it will be checked, whether there is one specified in the device description of the application..
 - 
                           
Afterwards the library profile will be checked for a resolution definition.
 - 
                           
The result is displayed in the Library Manager below the “Effective Version”.
 
A placeholder library, which is included in the “POUs” view, gets resolved as follows:
- 
                           
A specific resolution defined in the dialog “Placeholder” will be ignored.
 - 
                           
For the application it will be checked whether there is a resolution defined in the device description.
 - 
                           
Afterwards the library profile will be checked.
 - 
                           
The result is displayed in the tooltip of the
 symbol . 
Dialog box 'Placeholders'
| 
                                  “Name”  | 
                              
                                  Name of the placeholder.  | 
                           
| 
                                  “Library”  | 
                              
                                  Current resolution, valid for the project Double-click on the entry in order to edit the placeholder resolution. A selection list with the available library versions appears. Additionally the command “Other Library” is available.  | 
                           
| 
                                  Command “Other Library”  | 
                              
                                  The command opens the dialog box “Bibliothek durchsuchen” for searching and installing libraries. Choose this command, if you do not want to redirect to another version, but on a specific libray.  | 
                           
| 
                                  “Info”  | 
                              
                                  Type of placeholder resolution: 
  |