Function: This command loads the project source code (as project archive) to the controller.
Call: Main menu “File”.
Requirement: The network path for the controller must be configured.
After you execute the command, an overview opens with all devices in the network.
                     Select a controller from this overview. Then the Archiv.prj project archive is downloaded to this controller. You can click “Source Upload” to upload the complete source code to the CODESYS development system at a later time.
If you are already connected to a controller (in online mode), then the “Source Download to Connected Device” command is also available for this process.