Symbol 
Function: This command updates all inconsistent IDs in a static text list.
Call: Main menu “Textlist Paste Text”, context menu
Requirement: The “GlobalTextList” is open and active. A field in the table is selected. The object is write protected.
If CODESYS finds during checking that the global text list and the static texts of the visualizations do not correspond, this could be because the global text list is or was write protected. The requirement for this is that you have set up a user management system in the project.