Symbol: 
Function: This command scales the y-axis of the trace diagram for optimum display of all graphs, making sure that the y-values fit in the visible region of the diagrams. The command works with both single-channel and multi-channel displays.
Call: Menu bar: “Trace”; context menu.
Trace in a single-channel display
When all trace variables are displayed in one diagram, the trace is in single-channel display.
Trace in a multi-channel display
When the trace variables are displayed in multiple diagrams, the trace is in multi-channel display.