Symbol: 
Function: This command transfers the trace configuration on the controller to the associated application, and starts the data recording. The recorded data is transferred back to the development system. The trace diagram shows the current samples and continues.
Call: Menu bar: “Trace”; context menu.
Requirement: The command is available when the assigned application is in online mode.
See also