Symbol:
(command disabled),
(command enabled)
Function: This command enables and disables mouse zooming in the trace diagram.
Call: Menu bar: “Trace”; context menu.
User input in the trace diagram
If the command is enabled, then you can stretch a box with the mouse. When you release the mouse button, the display zooms in on the box and the data is enlarged.
See also