Symbol: 
Function: This command starts the data recording on the controller when it is stopped.
Call: Main menu “Trace”, or context menu.
Requirement: The assigned application on the runtime system is running and a trace configuration is loaded.
See also