Function: The dialog is used to display or change the properties of the selected breakpoint in the “Breakpoints” view.
Call:
- 
                           
“Breakpoints” view,
 “Properties” button  - 
                           
“Breakpoints” view,
“New” button, “New Breakpoint” command or “New Data Breakpoint” command 
Requirement: An entry is selected in the list of breakpoints.
The dialog is identical to the “New Breakpoint” dialog which is opened in the “Debug” menu by means of the respective commands. Therefore, see the description in the help for the “New Breakpoint” dialog.
See also