Function: The dialog defines how references to devices that are no longer available are to be handled.
Call: When opening a CoDeSys V2.3 project in V3, the dialog opens when the converter detects a device reference which cannot be used anymore.
A CoDeSys V2.3 project can be converted into a CODESYS V3 project only if the CODESYS V2.3 Converter package is installed in CODESYS V3. The package is available in the CODESYS Store.
| 
                                  “Use the following device that has already been installed”  | 
                              
                                  CODESYS replaces the previously used device in the device tree with another device. The “Browse” button opens a dialog for selecting from the local device repository.  | 
                           
| 
                                  “Ignore the device. All device specific objects will not be available in the new project”  | 
                              
                                  The device entry with all objects inserted below it is removed from the device tree.  | 
                           
| 
                                  “Remember this mapping for all future occurrences of that device”  | 
                              
                                  The settings made here in the dialog are saved in the CODESYS Options, in the “CODESYS V2.3 Converter” category. As a result, they are also valid for future project conversions.  |