Function: This dialog restricts the range of array elements whose values are displayed during monitoring.
Call: Click in the column field “Data Type” that belongs to the array variable.
Requirement: A POU is in online mode and is being monitored. In addition, a variable of the POU has the data type “ARRAY”.
| 
                                  “Valid range”  | 
                              
                                  The validity range of the array elements that are monitored. Example of a three-dimensional array:   | 
                           
| 
                                  “Maximum number of array elements”  | 
                              
                                  Number of elements of the array variables Example:   | 
                           
| 
                                  When you edit one of the settings “Start”, “End”, or “Scroll range of 1000 elements”, both of the other settings are adapted automatically.  | 
                           |
| 
                                  “Start”  | 
                              
                                  Index of the first array element whose value is displayed.  | 
                           
| 
                                  “End”  | 
                              
                                  Index of the last array element whose value is displayed.  | 
                           
| 
                                  “Scroll range of 1000 elements”  | 
                              
                                  Scrollbar for selecting a range from the set of array elements.  |