Symbol: 
Function: You use this dialog for storing the authentication data for the proxy server which is currently used for accessing the internet from CODESYS.
Call: Main menu “Tools Options”, category “Proxy Settings”
Requirement: Internet access of the network via proxy server
|
“Enter proxy credentials” |
A double click opens the input request for the user name and the password for the proxy server. CODESYS uses the access data for the establishment of the connection to the download server for libraries and the device description, for the establishment of the connection to the CODESYS Store and for the command “View Start Page”. Requirement: If the internet access of your computer or of the network takes place via a proxy server, then the button is available. |