Symbol: 
Function: The dialog contains settings for displaying and working in a text editor.
Call: Menu bar: “Tools Options”, category “Text editor”
Tab 'Theme'
On this tab, you set the desired theme in the interface design of the ST editor.
| 
                                  “Theme”  | 
                              
                                  Color theme for the text editor. The selected theme is shown in the “Preview” window. The available color schemes are stored in the installation directory in the
                                      | 
                           
Tab 'Editing'
| 
                                  “Number of undos”  | 
                              
                                  Maximum number of editing steps that you can apply the “Edit Undo” command to.  | 
                           
| 
                                  “Folding”  | 
                              
                                  Defines the structuring of the code by indentation. When you select an indentation, you can expand or collapse the indentation section by means of a plus and minus sign in front of the first line of each section. 
 ![]()  | 
                           
| 
                                  “Word wrap”  | 
                              
                                 
  | 
                           
| 
                                  “ Tab width”  | 
                              
                                  Number of characters  | 
                           
| 
                                  “Keep tabs”  | 
                              
                                  
  | 
                           
| 
                                  “Indent width”  | 
                              
                                  If you have selected “Smart” or “Smart with code completion” for the “AutoIndent” option, then CODESYS inserts the number of spaces at the beginning of the line.  | 
                           
| 
                                  “AutoIndent”  | 
                              
                                 
  | 
                           
Tab 'Text Area'
| 
                                  “Highlight current line”  | 
                              
                                  
  | 
                           
| 
                                  “Matching brackets”  | 
                              
                                  
  | 
                           
| 
                                  “End of line markers”  | 
                              
                                  
  | 
                           
| 
                                  “Wrap guide”  | 
                              
                                  
  | 
                           
| 
                                  “Font”  | 
                              
                                  Clicking the field opens the default dialog for configuring the font.  | 
                           
Tab 'Margin'
| 
                                  Settings for the left margin of the text editor window, which is separated from the input area by a vertical line:  | 
                           |
| 
                                  “Line numbering”  | 
                              
                                  
  | 
                           
| 
                                  “Highlight current line”  | 
                              
                                  
  | 
                           
| 
                                  “Show bracket scope”  | 
                              
                                  
  | 
                           
| 
                                  “Mouse Actions”  | 
                              
                                  You can assign one of the following actions to each of the specified mouse actions or mouse-keyboard combinations. CODESYS performs the selected action when you move the mouse to the plus or minus sign in front of the header of a bracketed area: 
  | 
                           
Tab 'Monitoring'
| 
                                  Settings for displaying the monitoring fields  | 
                           |
| 
                                  “Enable inline monitoring”  | 
                              
                                  
  | 
                           
| 
                                  “Number of displayed digits”  | 
                              
                                  Number of comma places in the monitoring field  | 
                           
| 
                                  “String length”  | 
                              
                                  Maximum length of string variable values in the monitoring field  | 
                           
See also

: