Function: This dialog box is used for preparing a value for a forced variable. CODESYS executes the prepared action with the next forcing.
CODESYS opens the dialog box in the following situations:
-
When clicking in the field “Prepared value” of a forced variable in the declaration section
-
When clicking in the inline monitoring field of a forced variable
-
When clicking in the field “Prepared value” of a forced variable in the monitoring window
|
“Prepare a new value for the next write or force operation” |
Value that CODESYS writes to the variable with the next force operation |
|
“Remove a preparation with a value” |
CODESYS deletes the prepared value. |
|
“Release the force, without modifying the value” |
CODESYS retains the forced value and ends forcing. CODESYS marks the variable |
|
“Release the force and restore the variable to the value it had before forcing it” |
CODESYS resets the forced value and ends forcing. The variable is marked with |
See also