Symbol: 
Function: This dialog is used for configuring the settings of SFC objects. The properties of each new SFC object automatically have the configured settings.
Call: Menu bar: “Project Project Settings” (“SFC”).
Requirement: A project is open.
Tab 'Flags'
| 
                                  Implicitly generated variables for checking and monitoring the processing in an SFC diagram  | 
                           |
| 
                                  “Active”  | 
                              
                                  
  | 
                           
| 
                                  “Declare”  | 
                              
                                  
  | 
                           
| 
                                  “Apply to all”  | 
                              
                                  In this dialog, CODESYS applies changes to existing SFC objects. CODESYS selects the “Use defaults” check box in the properties of the SFC POUs.  | 
                           




NOTICE

Automatically declared variables are visible in the declaration part of the SFC editor only in online mode.
Tab 'Build'
| 
                                  “Calculate active transitions only”  | 
                              
                                  
  | 
                           
| 
                                  This part of the dialog is available only for compiler versions < 3.4.1.0.  | 
                           |
| 
                                  “Company ” “Title” “Version”  | 
                              
                                  Defines the SFC library that CODESYS uses by default.  | 
                           
| 
                                  “Namespace”  | 
                              
                                  Enables unique references to libraries. Required when various versions of the library
                                    are available on the system. Please make sure that there are no discrepancies between
                                    the namespace defined in the library manager and the namespace defined for the individual
                                    object. The   | 
                           
Each SFC block stores the information via the library version that applied when you
                           added the block. This can cause you to use multiple library versions within the same
                           project. In order to prevent this, you are prevented from defining specific versions
                           of IecSfc.library (as of compiler version 3.4.1.0). The library version, which you use for all SFC
                           blocks in the project, is defined with a placeholder. CODESYS resolves the placeholder depending on the compiler version in use. The allocation
                           of the library version to the compiler version is defined in the library profile.
: The corresponding variable is used.