Symbol: 
Function: This dialog box is for configuring the compiler options.
Call: Main menu “Project Project Settings” (“Compileoptions” category).
Requirement: A project is open.
|
“Fix Version” |
Defines the compiler version that CODESYS uses when compiling and downloading for compile (for example, “3.5.6.0” for version 3.5 SP6). |
|
“Allow unicode characters for identifiers” |
Cleared by default because using Unicode characters in identifier names is not permitted in the IEC standard. May be required for some foreign languages (for example, Asian languages). |
|
“Replace constants” |
|
|
“Enable logging in breakpoints” |
For breakpoints that are defined as execution points, you can create a message text in the “Execution point settings” dialog box. CODESYS prints this text to the device log when the application halts at the execution point. |
|
“Maximum number of warnings” |
Refers to the warnings that CODESYS prints to the messages view. You define the selection of displayed compiler warnings in the “Project Settings” dialog box in the “Compiler Warnings” category. |
(default):
: Access to constants is possible, but it prolongs the computation time.