Symbol: 
Function: This dialog defines the layout for the print version of the project contents. This layout is used for the printout of the project information by clicking “File Print” and the printout of the project documentation by clicking “Project Document”.
Call: Main menu “Project Project Settings” (“Page Setup”)
You can change settings the following:
- 
                           
“Paper”
 - 
                           
“Margins”
 - 
                           
“Header and Footer”
 - 
                           
“Document”
 - 
                           
“Title Page”
 
| 
                                  The headers and footers are structured in table style. You can configure rows and columns, and add text and images to the resulting cells.  | 
                           |
| 
                                  “Row spanning”  | 
                              
                                  Number of rows that CODESYS should merge into a single column.  | 
                           
| 
                                  “Column spanning”  | 
                              
                                  Number of columns that CODESYS should merge into a single row.  | 
                           
![]()  | 
                              
                                  Opens the list of available placeholders for the “Text” field. When printing the page, CODESYS provides the placeholders with the current values.  |