Symbol: 
Function: this dialog is for the configuration of the project protection by a password, a dongle, or a certificate.
Call: Menu bar: “Project Project Settings” (category “Security”).




NOTICE

If the encryption password is lost you can no longer open the project. You can also no longer restore it.
| 
                                  “No protection”  | 
                              
                                  
 Note: We strongly recommend that you use security functionality. 
  | 
                           
| 
                                  “Integrity check”  | 
                              
                                  When you create a new project, this option is enabled by default. 
 Please note that the project file is not encrypted. To better protect your data, activate one of the encryption functions.  | 
                           
| 
                                  “Encryption”  | 
                              
                                  
  | 
                           
| 
                                  “Password”  | 
                              
                                  Entering, changing and confirming the encryption password. If you save the project with these settings you must enter the password later in order to open the project again, even if it is to be loaded as a library reference.  | 
                           
| 
                                  “Dongle”  | 
                              
                                  Requirement: you have connected the CODESYS security key (dongle) to the computer. “Add”: The dialog “Add Registered Dongle” opens.  | 
                           
| 
                                  “Registered dongles”  | 
                              
                                  Drop-down list of the registered dongles.  | 
                           
| 
                                  “Certificates”  | 
                              
                                  Certificates are used for the encryption of contents of the open project file. Requirement: The certificates for all users who share the project must be installed in the local memory. 
  | 
                           
| 
                                  “Dongle”  | 
                              
                                  Drop-down list of all connected dongles.  | 
                           
| 
                                  “Update”  | 
                              
                                  CODESYS refreshes the drop-down list.  | 
                           
| 
                                  “Flash”  | 
                              
                                  The LEDs of the currently selected dongle flash for two seconds (if it supports this function).  | 
                           
The dongle must be connected to the computer when CODESYS loads the project, even if it is loaded as a library reference.
: The project file is not protected from unauthorized access and data manipulation.
                                    
: The