Symbol: 
Function: This dialog activates the tests that the light version of CODESYS Static Analysis performs each time code is generated.
Call: Menu bar: “Project Project Settings” (“Static Analysis Light” category).
You can exclude lines of code from the static code analysis by marking the code with
                           the pragma {analysis ...} or the pragma {attribute 'analysis' := '...'}.
Additional compile tests
| 
                                  “SA0033: Unused variables”  | 
                              
                                  Finds variables that are declared, but not used within the compiled program code. For GVL variables: If there are multiple applications in one project, then only the
                                    objects under the currently active application are affected. If there is only one
                                    application, then the objects in the   | 
                           
| 
                                  “SA0028: Overlapping memory areas”  | 
                              
                                  Detects the locations where two or more variables reserve the same storage space.
                                    For example, this occurs for the following declarations:   | 
                           
| 
                                  “SA0006: Write access from multiple tasks”  | 
                              
                                  Detects variables that are written by more than one task.  | 
                           
| 
                                  SA0004 “Multiple write access on output”  | 
                              
                                  Detects outputs that are written to more than one location. Note: No error is reported when an output variable ( Note: A pragma cannot deactivate this rule.  | 
                           
| 
                                  “SA0027: Multiple use of identifiers”  | 
                              
                                  Detects multiple uses of a name/identifier for a variable or an object (POU) within the scope of a project. The following cases are detected: 
  | 
                           
| 
                                  “SA0167: Temporary function block instances”  | 
                              
                                  The test detects function block instances that are declared as temporary variables.
                                    This concerns instances that are declared in a method or in a function or as   | 
                           
Examples
SA0003: Empty statements
; (* Comment *); iVar;
SA0006: Concurrent access
FUNCTION_BLOCK ADD_FB g_iTemp1 := g_iTemp1 + INT#1;
PROGRAM PLC_PRG //controlled by MainTask g_iTemp1 := g_iTemp1 + INT#2; g_xTemp2 := g_iTemp1 > INT#10;
PROGRAM PLC_PRG_1 //controlled by SubTask g_iTemp1 := g_iTemp1 - INT#3; g_xTemp2 := g_iTemp1 < INT#-10;
SA0004 Multiple write access on output
VAR_GLOBAL
    g_xVar AT %QX0.0 : BOOL ; 
    g_iTest AT %QW0 : INT ;
END_VAR
                     PROGRAM PLC_PRG
IF iCondition < INT#0 THEN
    g_xVar := TRUE;
    g_iTest := INT#12;
END_IF
                     CASE iCondition OF
    INT#1:
        g_xVar := FALSE;
    INT#2:
        g_iTest := INT#11;
    ELSE
        g_xVar := TRUE;
        g_iTest := INT#9;
END_CASE
 
                     SA0006: Write access from multiple tasks
FUNCTION_BLOCK ADD_FB g_iTemp1 := g_iTemp1 + INT#1; PROGRAM PLC_PRG // Controlled by MainTask g_iTemp1 := g_iTemp1 + INT#2; g_xTemp2 := g_iTemp1 > INT#10; PROGRAM PLC_PRG_1 //Controlled by SubTask g_iTemp1 := g_iTemp1 - INT#3; g_xTemp2 := g_iTemp1 < INT#-10;
SA0027: Multiple use of name
PROGRAM PLC_PRG VAR ton : INT; // error SA0027 END_VAR
SA0029: Different notation in implementation and declaration
The PLC_PRG POU and a fnc function POU are in the device tree.
PROGRAM PLC_PRG VAR iVar:INT; _123test_var_: INT; END_VAR ivar := iVar + 1; // notation different to that in the declaration part -> SA0029 _123TEST_var_ := _123test_var_INT; // notation different to that in the declaration part -> SA0029 Fnc(); // notation different to that in the devices tree -> SA0029 END_VAR
SA0167: Temporary function block instances
PROGRAM PLC_PRG
VAR
END_VAR
VAR_TEMP
    yafb: AFB;   
END_VAR
FUNCTION Fun : INT
VAR_INPUT
END_VAR
VAR
    funafb: AFB;
END_VAR
METHOD METH: INT
VAR_INPUT
END_VAR
VAR
    methafb: AFB;
END_VAR
                     See also