Symbol: 
Function: The dialog enables the setting of the visualization profile.
Call: Menu “Project Project Settings”, category “Visualization Profile”
Requirement: A project is open.
| 
                                  “Certain profile”  | 
                              
                                  Profile that CODESYS uses in the project and that determines the visualization elements that are available in the project. The selection list contains all the profiles installed so far.  |