Function: The settings on this tab define when and how a boot application is created from the application.
Requirement: The device supports the settings.
Call: Select the application object; context menu: “Properties”; menu bar: “View Properties”, “Boot Application” category
| 
                                  “Create implicit boot application on download”  | 
                              
                                  A boot application is created automatically when downloading the application.  | 
                           
| 
                                  “Create implicit boot application on Online Change”  | 
                              
                                  A boot application is created automatically when for an online change.  | 
                           
| 
                                  “Remind boot application on project close”  | 
                              
                                  Before closing the project, CODESYS prompts to create the boot application.  | 
                           
| 
                                  “Verify boot application after creation”  | 
                              
                                  After the boot application is created, an independent service checks whether or not the boot application has been created correctly.  | 
                           
Regardless of the presets defined here, you are always able to create a boot application explicitly when you login.
See also