Symbol: 
Function: The dialog contains options for building (build operation) the object.
Call: Menu bar: “View Properties”; context menu of the object in the device tree
|
Name |
Description |
|---|---|
|
“Exclude from build” |
The object entry is displayed in green fonts in the “Devices” or “POUs” view. |
|
“External implementation” “(Late link in the runtime system) ” |
The object name is postfixed with |
|
“Enable system call” |
Background: As opposed to CoDeSys V2.3, the ADR operator in V3 can be used with function names, program names, function block names, and method names. It replaces the INSTANCE_OF operator. BUT: It is not possible to call function pointers from within CODESYS. |
|
“Link always” |
Note: The pragma |
|
“Compiler defines” |
Here you can specify defines or conditions for compiling the object (conditional compile).
You can also type in the expression Example: |
|
“Additional compiler definitions from the device description” |
|
|
“Defined in device” |
List of compiler definitions that originate from the device description. These compiler definitions are used in the build if they are not listed in the “Ignored definitions” field. |
|
“Ignored definitions” |
List of compiler definitions from the device description that are not used in the build. |
|
|
Copies the selected compiler definition from the “Defined in device” field to the “Ignored definitions” field. |
|
|
Moves the selected compiler definition from the “Ignored definitions” field to the “Defined in device” field. The compiler definition is used in the build. |
: This object and recursively its child objects are not considered for the next compile
process.