Function: The dialog allows for setting the basic properties of the selected image pool.
Call: “View Properties” of an “Image Pool” object type; context menu of an “Image Pool” object type.
| 
                                  “Download only used images”  | 
                              
                                  
  | 
                           
| 
                                  “Download by visualization”  | 
                              
                                  
  | 
                           
| 
                                  “Internal”  | 
                              
                                  
  | 
                           
| 
                                  “Mark library as symbol library”  | 
                              
                                  Marks the image pool as a symbol library for use in a visualization. The symbol library
                                    receives the key  Requirement: A library project is open. CODESYS displays symbol libraries that are installed in the repository in the “Project Settings” (“Visualization” category, “Symbol Libraries” tab).  | 
                           
| 
                                  “Textlist for symbol translation”  | 
                              
                                  Select the text list from the drop-down list that contains the translated texts for the image pool.  | 
                           
: Instead of loading all images from the image pool,