Function: This dialog box includes the configuration for buffering the trend data of a trend recording.
Call: “Trend Storage” button in the editor of a trend recording.
|
“Maximum number of variables” |
Maximum number of trend variables that can be managed in the database. If you increase this value afterwards, then will CODESYS perform a download and reconfigure the database. |
|
“Store every N milliseconds” |
Time interval (in ms) when the A high value results in better runtime performance. The disadvantage is the increased risk of losing data if the controller crashes or shuts down. A low value reduces this risk. The disadvantage is the slower control over a trend visualization with large amounts of data. |
|
“Limit” |
|
: Limit the recording
) of the drop-down list will set the units to kilobytes (KB), megabytes (MB), or gigabytes
(GB).