This tab of the generic device editor includes a text-based control monitor for querying specific information from the controller. You can specify device-dependent commands for this and receive the response from the controller in a result window.
|
Command with Possible Parameters |
Description |
|---|---|
|
? |
List of available PLC shell commands with possible parameters and short description |
|
|
Provides a list of all loaded applications The order in the list defines the application index beginning with |
|
|
Get battery status; |
|
|
handle logging data in case of crash or malfunction; |
|
|
Generates CSR files for all applications |
|
|
Exports the specified certificate |
|
|
Generates self-signed certificates The validity period of the certificate can be specified by means of Default value: 365 days |
|
|
Generates the parameters for the Diffie-Hellman key exchange Caution: This operation can take several minutes to complete. |
|
|
Provides all registered and used certificates (ID of the component and usage). |
|
|
Lists all certificates of the specified trust level If a trust level is not given, then all certificates are listed. Possible trust levels
|
|
|
Imports the specified certificate |
|
|
Removes the specified certificate |
|
|
Provides information about the communication channel |
|
|
Init and mark SRAM segment or complete SRAM as free |
|
|
Get version information of communication modules |
|
|
Get information of serial COM ports |
|
|
Shows the processor load of the CPU (for multicore, each processor core) |
|
|
Get/set system date;
|
|
|
Will show Ethernet information; |
|
|
List of names of available PLC shell commands |
|
|
Shows whether or not multicore is supported and the number of available processor cores |
|
|
- |
|
|
Provides the program status of the given application, or the program status of all loaded applications if no application is given |
|
|
Display layout of complete SRAM |
|
|
Provides a list of all task groups, their tasks, and the CPU core binding |
|
|
Provides a list of defined task groups The assigned tasks are shown for each task group. |
|
|
Get list of all tasks, its name and the optional bound taskgroup |
|
|
Print memory usage and heap statistics |
|
|
Will show I/O bus information; |
|
|
License handling commands; |
|
|
Provides the GUID (application index) of one or all loaded applications |
|
|
Provides the contents of the following fields from the project information: title, version, author, and description. Requirement: The option “Create POU for properties access automatically” in the “Project Information” dialog is activated. |
|
|
Shows the processor load of the controller (in percent) |
|
|
Get production data and public keys information of CPU |
|
|
Performs PLC reboot |
|
|
Repeats the given command (for testing the connection) |
|
|
Loads the boot application of the given application, or the boot projects of all loaded applications if no application is given |
|
|
Resets the given application, or all loaded applications if no application is given |
|
|
Executes a cold boot of the given application, or all loaded applications if no application is given |
|
|
Restore retains to files(s). [Optional only from specified application]. |
|
|
Restore complete SRAM content to file |
|
|
Provides the universal time (UTC) via the |
|
|
Sets the universal time (UTC) via the |
|
|
Provides information about the runtime system, for example the processor and version of the runtime system |
|
|
Get version errors from DPRAM from communication module <slot> |
|
|
Save retains to files(s). [Optional only from specified application]. |
|
|
Save complete SRAM content to file |
|
|
Clone content of SM560-s at slot <slot> |
|
|
Provides the number of currently logged in clients/users |
|
|
Provides a list of all currently logged in clients/users |
|
|
Show the list of all security settings and the current configuration |
|
|
Export or import data from SRAM |
|
|
Starts the given application, or all loaded applications if no application is given |
|
|
Stops the given application, or all loaded applications if no application is given |
|
|
Get/set system time;
|
|
|
Configure location of the trend DB, reboot of CPU and download is required |
|
|
Get version information on AC500 components |
* Application name: Name of the application in the device tree
Application index: Results from the list of all applications on the controller that
you can call with the “applist” command. Index 0 stands for the first application in the list, 1 for the second, and so on.