Symbol: 
Implement more program code in an action. You can implement this program code as the base implementation in another language. The base implementation is a function block or a program where you inserted the action.
An action does not have its own declaration and it works with the data from the base implementation. This means that the action uses the input and output variables and the local variables from its base implementation.
Add an “Action” to a function block or program by clicking “Project Add Object Action”.
|
“Name” |
Name of the action |
|
“Implementation language” |
List box of implementation language |
Input support when generating inheriting POUs
When you doing object-oriented programming and using the inheritance (keyword EXTENDS) of POUs, you can get support as follows:
When you insert an action, a property, a method, or a transition below a POU derived from a base POU, the “Add …” dialog opens. Then the input field for the name extends to a list box. The list box contains a valid selection from the actions, properties, methods, or transitions available in the base POU. Now you can, for example, easily accept a method of the base POU and then adapt it to the derived function of the POU.
Methods and properties with the access modifier PRIVATE are not listed here because they are also not inherited. Methods and properties with
the access modifier PUBLIC automatically get a blank access modifier field when accepting into the derived POU,
which means the same thing functionally.
Example

Calling an action
Syntax:
<program>.<action> or <FB instance>.<action>
To call an action from only within the base implementation, you only have to provide the action name.
Examples
Calling a “Reset” action from another POU The call is not executed from the base implementation.
Declaration:
PROGRAM PLC_PRG
VAR
Inst : Counter;
END_VAR
Calling a “Reset” action from an IL POU
CAL Inst.Reset(In := FALSE) LD Inst.Out ST ERG
Calling a “Reset” action from an ST POU
Inst.Reset(In := FALSE); Erg := Inst.out;
Calling a “Reset” action from an FBD POU

Actions are used frequently in the SFC implementation language.
See also
-
linktarget doesn't exist but @y.link.required='true'