Symbol: 
This object is used to create, manage, and translate texts. It contains a table with texts where you can add new texts. You can select a text which you have composed here can be selected in a visualization in the “Dynamic texts” property of an element. In runtime mode, the visualization displays this text dynamically in the selected language.
When the object is assigned to an alarm group and is located below the “Alarm Configuration” object, CODESYS adds the texts of the alarm group to the table. You can also add texts.
|
“ID” |
Unique identifier of the text |
|
“Standard”: |
Source text as character string (example: Double-click in the field to edit the text. |
|
The table contains as many language columns as you want to add. A language column is named with a language code that you specified when you created the column by means of the “Insert Language” command. |
|
|
“<language code>” |
Name of the language as a language code. Example: |
|
Blank line |
Edit the line to add your own text. |
See also
-
For descriptions about alarm management and alarm visualization, see the help for CODESYS Visualization.