This operator is an extension of the IEC 61131-3 standard.
You can use this operator to dereference pointers by appending the operator as ^ to the pointer identifier. 




CAUTION

When using pointers to addresses, please note that applying an online change can shift address contents.
Example
ST:
pt : POINTER TO INT; var_int1 : INT; var_int2 : INT; pt := ADR(var_int1); var_int2 := pt^;