The pragma provides an estimated value for the stack size requirement.
Methods with recursive calls cannot pass a stack check because stack usage cannot be determined. As a result, a warning is issued. To prevent this warning, you can give the method an estimated value (in bytes) for the stack size requirement. Then the method passes the stack check successfully.
Syntax
{attribute 'estimated-stack-usage' := '<estimated stack size in bytes>'}
Example
{attribute 'estimated-stack-usage' := '127'} // 127 bytes
METHOD PUBLIC DoIt : BOOL
VAR_INPUT
END_VAR
Insert location: First line above the declaration part of the method.
The section "Method call" includes an example that uses this pragma.
Recursive method call
Within its implementation, a method can call itself, either directly by means of the
THIS pointer, or by means of a local variable for the assigned function block.
Use recursions mainly for processing recursive data types such as linked lists. In general, we recommend to be careful when using recursion, as unexpectedly deep recursions can cause stack overflow and machine downtime.
Example
Calculation of the factorial
The following program PLC_PRG calculates the factorial of a number in the FB_Factorial function block in a different way, each in its own method.
-
Method
m_Iterative: Iterative -
Method
m_Pragmaed: Recursive with warning suppression -
Method
m_Recursive: Recursive -
Method
m_Temp: Temporary with warning suppression
A warning is issued for the m_Recursive method only.

// Contains the data of the factorial calculation of uiNumber
TYPE FACTORIAL_RESULT :
STRUCT
uiNumber : UINT;
udiIterative : UDINT;
udiRecursive : UDINT;
udiPragmaed : UDINT;
udiTemp : UDINT;
END_STRUCT
END_TYPE
PROGRAM PLC_PRG
VAR
fb_Factorial_A : FB_Factorial;
factorial_A : FACTORIAL_RESULT := (uiNumber := 9, udiIterative := 0, udiRecursive := 0, udiPragmaed := 0 );
END_VAR
fb_Factorial_A.p_Number := factorial_A.uiNumber;
factorial_A.udiIterative := fb_Factorial_A.m_Iterative();
factorial_A.udiRecursive := fb_Factorial_A.m_Recursive(uiN := factorial_A.uiNumber);
factorial_A.udiPragmaed := fb_Factorial_A.m_Pragmaed(uiN := factorial_A.uiNumber);
factorial_A.udiTemp := fb_Factorial_A.m_Temp(uiN := factorial_A.uiNumber);
//Factorial calculation in different ways
FUNCTION_BLOCK FB_Factorial
VAR_INPUT
END_VAR
VAR_OUTPUT
END_VAR
VAR
uiN : UINT;
udiIterative : UDINT;
udiPragmaed : UDINT;
udiRecursive : UDINT;
END_VAR
// Iterative calculation
METHOD PUBLIC m_Iterative : UDINT
VAR
uiCnt : UINT;
END_VAR
m_Iterative := 1;
IF uiN > 1 THEN
FOR uiCnt := 1 TO uiN DO
m_Iterative := m_Iterative * uiCnt;
END_FOR;
RETURN;
ELSE
RETURN;
END_IF;
//Recursive calculation with suppressed warning
{attribute 'estimated-stack-usage' := '99'}
METHOD PUBLIC m_Pragmaed : UDINT
VAR_INPUT
uiN : UINT;
END_VAR
VAR
END_VAR
m_Pragmaed := 1;
IF uiN > 1 THEN
m_Pragmaed := uiN * THIS^.m_Pragmaed(uiN := (uiN - 1));
RETURN;
ELSE
RETURN;
END_IF;
//Recursive calculation
METHOD PUBLIC m_Recursive : UDINT
VAR_INPUT
uiN : UINT;
END_VAR
VAR
END_VAR
m_Recursive := 1;
IF uiN > 1 THEN
m_Recursive := uiN * THIS^.m_Recursive(uiN := (uiN - 1) );
RETURN;
ELSE
RETURN;
END_IF;
// Called by temporary FB instance
{attribute 'estimated-stack-usage' := '99'}
METHOD PUBLIC m_Temp : UDINT
VAR_INPUT
uiN : UINT;
END_VAR
VAR
fb_Temp : FB_Factorial;
END_VAR
m_Temp := 1;
IF uiN > 1 THEN
m_Temp := uiN * fb_Temp.m_Temp(uiN := (uiN - 1));
RETURN;
ELSE
RETURN;
END_IF;
PROPERTY p_Number : UINT
uiN := p_Number; //Setter method
Only the m_Recursive issues a warning when the program is executed.