This pragma can be applied to a local STRING variable and causes this local STRING
                     variable to be initialized in sequence with the device tree path of the POU to which
                     it belongs. This can be useful for error messages. The application of the pragma requires
                     the application of the attribute 'reflection' to the associated POU, as well as the application of the additional attribute 'noinit' to the STRING variable.
Syntax:
{attribute 'instance-path'} 
Insertion position: the line above the line with the declaration of the STRING variable.
Example
The following function block contains the attributes 'reflection', 'instance-path' and 'noinit'.
{attribute 'reflection'}
FUNCTION_BLOCK POU
VAR
 {attribute 'instance-path'} 
 {attribute 'noinit'}
 str: STRING;
END_VAR
                     An instance “myPOU” of the function block “POU” is defined within the main program “PLC_PRG”:
PROGRAM PLC_PRG VAR myPOU:POU; myString: STRING; END_VAR myPOU(); myString:=myPOU.str;
Following the initialization of the instance myPOU, the path of the instance myPOU is assigned to the string variable str, in the example PLCWinNT.Application.PLC_PRG.myPOU. This path is assigned in the main program to the variable myString.




NOTICE

You can define the length of a string to be whatever you like (even >255), but you must consider that the string will be truncated at the end if it is assigned to a variable whose data type is too small for it.