CODESYS provides the capability to display the events and error messages logged in the controller.
See also
Reading the log
Requirement: The controller is running.
- 
                           
Select the controller in the device tree.
 - 
                           
Choose the command “Project Edit Object”.
The device editor opens.
 - 
                           
Choose the tab “Log”.
 - 
                           
Click on
 to update the view.A connection to the controller is established. The controller in the device tree is highlighted in green.
All controller log information are displayed.
 - 
                           
Click on
 to delete the current list. - 
                           
Filter the view by clicking on the desired category (for example "Information").
 - 
                           
Save the log entries. Click on
 and choose a file name. 
See also