In general, refactoring is a technique for improving the design of existing software code without changing the way it functions.
In CODESYS, refactoring provides functions for renaming objects and variables and updating referenced pins. You can display all occurrences of renamed objects and variables and then rename them all at once or individually. In “Tools Options”, you can also configure where CODESYS will prompt you for refactoring.
Renaming global variables
Requirement: A project is open that includes at least a function block “FB” and a global variable list. The global variable list “GVL” is open in the editor and contains a variable declaration (example: iGlobal). “FB” uses iGlobal.
Renaming global variables throughout the project
-
Select the global variable name
iGlobal. -
Right-click the variable and click “Refactoring Rename iGlobal”.
-
In the “Rename” dialog, type a name in the “New name” input field, for example
iGlobalOK, and click “OK”.The “Refactoring” dialog opens. In the device tree view on the left, the “GVL” and “FB” objects are highlighted in red and yellow. In the view on the right, “FB” in is open in its editor and
iGlobalhas already been renamed asiGlobalOK. -
Click “OK”.
-
No global variable
iGlobalis in your project. NowiGlobalOKis everywhere.
Renaming global variables throughout the project (except for a POU)
-
Select the global variable name
iGlobal. -
Right-click the variable and click “Refactoring Rename iGlobal”.
-
In the “Rename” dialog, type a name in the “New name” input field, for example
iGlobalTest, and click “OK”.The “Refactoring” dialog opens. In the device tree view on the left, the “GVL” and “FB” objects are highlighted in red and yellow. In the window on the right, the function block “FB ” is open in its editor.
iGlobalTestis listed instead ofiGlobal. -
Right-click in the view on the right.
-
Click “Reject this Object” and click “OK”.
The global variable
iGlobalis available in “FB” in your project. The variableiGlobalTestis now specified in the objects where the previous variable occurred.The error message in the message view reports that the
iGlobalidentifier is not defined.
Adding and removing input variables
In the declaration part of blocks, you can add and delete input and output variables by using the refactoring commands. CODESYS performs updates at the occurrence locations and calling locations of the blocks. You can accept or reject these updates individually. The “Refactoring” dialog also opens for this purpose.
Requirement: The FCT (function type) POU is open in the editor. The function already contains the input
variables input1, input2, and inputx. They are called in the PLC_PRG and POU programs.
-
Set the focus in the declaration part of the FCT function.
-
Click “Refactoring Add Variable”.
The default dialog opens for declaring variables.
-
Declare the variable
input_3with the scope ofVAR_INPUTand data typeINT. Click “OK” to close the dialog.The “Refactoring” dialog opens (see figure below). The affected locations are marked in yellow. (1)+(2)
-
In the upper right corner, select “Add inputs with placeholder text” from the drop-down list. (3).
-
In the left side of the window, click one of the highlighted objects (for example,
PLC_PRG). Right-click and choose the “Accept Whole Project” command to add the new variable at the new location of use inFCTfor the entire project.You see the change in the implementation part of
PLC_PRGin the view on the right: The placeholder_REFACTOR_appears at the location where the new variable was added. -
Click “OK” to close the “Refactoring” dialog.
-
Click “Edit Find”. Search the project for "_REFACTOR_" to check and edit the affected locations.
-
Note: As an alternative, you can insert the new variable with another initialization value without working with a placeholder first. In this case, in Step 4 you select "Add inputs with the following value" and type the value in the field on the right side of the drop-down list.

Example of a new variable with placeholder text in a CFC block:

Please note that you can also remove variables with refactoring.
Reordering variables in the declaration
In the declaration part of function blocks, you can change the order of declarations
by refactoring This is possible for declarations with scope VAR_INPUT, VAR_OUTPUT, or VAR_IN_OUT.
Requirement: The declaration part of a POU is open and includes declarations, for example:
VAR_INPUT invar2 : INT; invar1 : INT; in : DUT; bvar : BOOL; invar3 : INT; END_VAR
-
Right-click in this declaration block to access the context menu.
-
Click “Refactoring Reorder Variables”.
The “Reorder” dialog opens with a list of
VAR_INPUTvariables. -
Drag the “invar1 : INT;” entry to the position before the “invar2.” entry.
The
invar1declaration is now at the top position. -
Click “OK” to close the dialog.
The “Refactoring” dialog opens. The affected locations are marked in yellow (see figure above).
-
Click “OK” to accept the new order for the function block.
Changing a variable declaration and applying refactoring automatically
Refactoring helps you in the declaration when renaming variables (by means of "Auto declare").
Requirement: Function block fb_A.
-
Click “Tools Options”.
The “Options” dialog opens.
-
Select the “Refactoring” category.
-
In “Auto-Declare”, activate the options “On renaming variables” and “On adding or removing variables, or for changing the namespace”.
-
Double-click the function block
fb_A. -
Select a variable in the declaration of
fb_A, for exampleiA. As an alternative, you can set the cursor before or in the variable. -
Specify “Edit Declare variable” ([Shift]+[F2]).
The “Declare Variable” dialog opens. The dialog includes the settings of
iA. -
Change the name of
iAtoiCounter_A. -
The option “Changes by means of refactoring” appears and is activated.
-
Click “OK”.
The dialog “Refactoring” “Renaming from iA to iCounterA” opens. All locations affected by the variable renaming are marked there.
-
Click “OK” to close the dialog.
The changes are applied.