| 
                                  Comment  | 
                              
                                  Description  | 
                              
                                  Example  | 
                           
|---|---|---|
| 
                                  Single-line  | 
                              
                                  There are two ways of marking: 
 In CODESYS, these comments are handled the same way. However, if library documentation is created using the LibDoc Scripting Collection, the following applies: 
  | 
                              
                                  
 
  | 
                           
| 
                                  Multiline  | 
                              
                                  Starts with   | 
                              
                                  
  | 
                           
| 
                                  Nested  | 
                              
                                  Starts with   | 
                              
                                  
  | 
                           
Comments for tooltips and POU documentation
A tooltip in the header of a POU is defined by the following comment:
    // tooltip text – line 1
    // tooltip text – line 2
    // tooltip text – line 3
    Afterwards the documentation is defined as follows:
    /// reStructuredText
                     Note: It is not recommended to mix the different comment types because this can cause unwanted side-effects when the documentation is generated.