CODESYS provides special POUs that implement implicit monitoring functions. At runtime, these functions check the array limits or subrange types, the validity of pointer addresses, or division by zero.
- 
                           
Select the “Application” object in the device tree.
Click “Project Add Object POU for Implicit Checks”
The “Add POU for Implicit Checks” dialog box opens.
 - 
                           
Select the desired functions.
 - 
                           
Click “Add”.
The selected POUs are inserted below the “Application” in the device tree.
 - 
                           
Open the POUs in the editor.
 - 
                           
Adapt the implementation suggestion to your requirements.




CAUTION

To obtain the feature for monitoring functions, do not edit the declaration section. However, you are permitted to add local variables.