Symbol: 
Function: The dialog “Background” opens. You can define here whether the background of the visualization is colored or displayed with an image.
Call: Menu “Visualization”, context menu
See also
Dialog 'Background'
|
“Use Color” |
Color defined as a style color or as a fixed value. |
|
“Use Image” |
Reference to an image from an image pool in the project, formally specified as an
instance path: Example:
|
: Background in color