Symbol:
; keyboard shortcut: [Alt]+[F6].
Function: This command opens and closes the “Keyboard Configuration” tab above the visualization editor.
Call: Menu bar: “Visualization”.
Requirement: A visualization is open and active in the visualization editor.
See also
Tab 'Keyboard configuration'
Symbol: 
This tab contains a list of keyboard shortcuts with an editing option.
A keyboard shortcut can refer specifically to an element. Then the configuration appears here and in the “Input configuration” property of the associated element.
A keyboard shortcut can also have several configurations. If a keyboard shortcut has multiple keyboard configurations, then its input actions are executed in the order listed here.
Keyboard shortcuts of the default keyboard action are not listed here.
|
“Key” |
Key that a keyboard configuration is defined. Example: [M] Note: You can combine the key with [Ctrl], [Alt], and/or [Shift]. |
|
“Key down” |
Double-click: Drop-down list of all keys. Note: If the input action should be executed for both pressing the key ( |
|
“Shift” |
|
|
“Ctrl” |
|
|
“Alt” |
|
|
“Action type” |
input action Double-click: Drop-down list of input actions. Tip: For a description of input actions, refer to the “Input configuration” dialog box. |
|
“Action” |
Configuration of the input action that was selected next. Double-click: A dialog box opens that varies according to the input action. It allows the user-prompted customization of the settings. Tip: For a description of dialog boxes, refer to the “Input configuration” dialog box. The input action is configured in the same way here. |
|
“Element ID” |
ID of the visualization element where the user can execute the key event. The ID is relevant only if the event is also assigned to an element. Tip: The assignment of ID to element name is listed in the “Element list”. |
|
“Access rights” |
Access privileges of the action per user group Requirement: The visualization has a user management. |
|
|
Clicking the symbol on the right of the list moves the selected row one line down. |
|
|
Clicking the symbol on the right of the list moves the selected row one line up. |
|
Blank line |
Allows adding a new keyboard configuration. |
: The input action is executed when the user presses the key.
: The input action is executed when the user releases the key.