Function: The command makes further commands available. They are for specifying the order of the elements in levels, since elements in the rear levels are concealed by those in the front levels.
Call: Menu “Visualization”, context menu
Requirement: The visualization elements are positioned behind one another.
Command 'Bring to Front'
Symbol: 
Function: The command positions the selected visualization element in the front level. The element becomes completely visible.
Call: Menu “Visualization Order”, context menu
Command 'Bring One to Front'
Symbol: 
Function: The command positions the selected visualization element one level further forwards.
Call: Menu “Visualization Order”, context menu
Command 'Send to Back'
Symbol: 
Function: The command positions the selected visualization element in the back level.
Call: Menu “Visualization Order”, context menu
Command 'Send One to Back'
Symbol: 
Function: The command positions the selected visualization element one level further backwards.
Call: Menu “Visualization Order”, context menu