Symbol: 
Function: When you execute this command in “Visualization”, the “Trend Wizard” dialog box opens.
Call: Menu bar: “Visualization”; context menu of a “Trend” element in the visualization editor.
Requirement: A trend is selected in the active visualization editor.
Dialog 'Trend wizard'
Each row of the table contains a control element that can assigned to the trend. The elements are placed in the visualization next to the trend. The control elements are saved in the “Assigned control elements” property and can be modified there.
|
“Attached control element” |
|
|
“Position” |
Position of the control element in relation to the trend. |
|
“Type of element to insert” |
Drop-down list with the installed types of the control element |
|
“Instance name” |
Instance name of the control element |
: The associated element is available in the visualization and connected with the
trend via the property
: Deactivating the option does not cause the element to be deleted from the visualization.