Function: The dialog is for setting the color gradient of visualization elements. If you define two colors, the color graduates between them. If you only select 1 color, the color graduates within this color through its brightness. The detailed settings are for a special specification of the initial position and the angle of the color gradient.
Call: Click in the value field of the property “Gradient settings”
Requirement: You have selected a visualization element in the editor that has the property “Gradient settings”.
|
“Gradient type” |
|
|
“Color 1” |
First color of the gradient. |
|
“Color 2” |
Second color of the gradient. |
|
“Transparency” |
Transparency of the associated color. Permissible values: Integers in the range of
values from |
|
“Standard linear” |
Requirement: “Linear” color gradient. Standard direction of the linear color gradient. |
|
“Standard radial” |
Requirement: “Radial” color gradient. Standard setting. |
|
“Standard axial” |
Requirement: “Axial” color gradient. Direction of the color gradient |
|
“Angle (degrees)”: |
Requirement: “Linear” or “Axial” color gradient. |
|
“Center X (%):” |
Requirement: “Radial” color gradient. X-position of the center point (0 – 100%) |
|
“Center Y (%):” |
Requirement: “Radial” color gradient. Y-position of the center point (0 – 100%) |
|
“Use one color” |
Color gradient between “Color 1” and the same color with a different brightness. |
|
“Brightness” |
Requirement: The option “Use one color” is selected. Setting from 0 (black) to 100 (white) |
|
“Use two colors” |
Color gradient between the two selected colors “Color 1” and “Color 2”. |