Symbol: 
Function: The object is used to configure the web-based display variant for remote display of the visualization of the controller in a web browser. This allows for remote access, remote monitoring, as well as service and diagnostics of an application over the Internet.
Requirement: The object is inserted below the Visualization Manager, and the target system has a web server with CODESYS WebVisu support. The web server allows for the communication between the target system and the web browser.
See also
|
“Start Visualization” |
Name of the visualization where the start is displayed as CODESYS WebVisu. Hint: Use the Input Assistant to select another visualization. |
|
“Name of the .htm file” |
Base URL of the web page. The URL is also specified as the address in the web browser. Example: Note: If you use a BeagleBone Black as a visualization device, then you have to note
that a BeagleBone Black uses port 9090 for its web server. A valid IP address is as
follows: |
|
“Use as default page” |
Example: Notice: Even if you have created multiple web visualizations, you can activate this option for exactly one web page only and therefore preset only one page as the default page. |
|
“Update rate (ms)” |
Refresh rate (in milliseconds) in the web browser |
|
“Default communication buffer size” |
Default size for communication buffer (in bytes). Defines the maximum available memory for data transfer between the web client and the web server. Example: |
|
“Show Used Visualizations” |
The link opens the “Visualizations” tab in the “Visualization Manager” editor. The tab provides information about the visualizations downloaded to the display variants. |
|
“Fixed” |
|
|
“Isotropic” |
|
|
“Anisotropic” |
|
|
“Use scaling options for dialogs” |
|
|
“Client height” |
Height of the visualization (in pixels). |
|
“Client width” |
Width of the visualization (in pixels). |
|
“Antialiased drawing” |
|
|
“Standard text input with” |
Effect: When you configure a user input for default text input, select an input configuration for input action “Write Variable”, and configure the “Input type” as “Default”, then the settings are used here. |
|
“Treat touch as mouse actions” |
|
: The page specified in
: Fixed size of the visualization. The values used are