The “Visualization Toolbox” view provides the following elements for selection:
-
All visualization elements which the set visualization profile defines.
-
Image elements for all images of the project from the integrated libraries or symbol libraries.
-
Frame elements for all visualizations of the project or from the libraries.
See the “Project Settings” for the currently set visualization profile and the currently used symbol libraries.
The elements are combined into specific categories, each of which has its own button in the “Visualization Toolbox” view. You can create new categories and assign its elements.
The elements of the categories are displayed in the “Visualization Toolbox” view as preview images. It is also possible to search for an element name.
Simply drag the preview image of the element to the desired position in the editor window. Then the configurable properties of the element are displayed automatically in the “Properties” view of the visualization editor.
Create or remove new element category
Requirement: The visualization editor is open.
-
In the “Visualization Toolbox” view, click the
button.the “Configure Categories and Items” dialog opens.
-
In the dialog, click the
symbol to open the “Add Category” dialog. Note: Click the
symbol or press the [Del] key to delete the definition of a category. -
In the “Name” field, specify a name (example:
tagA) and click “OK” to close the dialog.In the “Configure Categories and Items” dialog, the new custom category
tagAis inserted below in the tree view. It is provided with the
symbol. -
Click the “Enable” option for the new category, and click “OK” to close the dialog.
CODESYS adds a “tagA” button in the “Visualization Toolbox” view. When you click the button, all elements that are assigned to this category are displayed.
Assigning a visualization element of an element category
Requirement: The visualization editor is open. You have already created a custom category
tagA. A button labeled tagA is visible in the “Visualization Toolbox” view.
-
In the “Visualization Toolbox” view, right-click an element to open its context menu.
A context menu opens. It contains the “Add Item to Category 'tagA'” and “Add to Categories” commands.
-
Click “Add to Category 'tagA'” and click “OK” to close the dialog.
-
Click the “tagA” button.
All elements are displayed which are assigned to this category, below it also the currently assigned element.