IL can be enabled in the CODESYS options if required: In the ⮫ “Dialog: Options: FBD, LD and IL ” dialog, on the “IL” tab, select the “Enable IL” option.




CAUTION

Data loss: An error-free conversion requires code which has correct syntax. Otherwise parts of the implementation can be lost.
Shortcut: [Ctrl]+[3]
Function: The command converts the active function block code or the active ladder diagram into an instruction list.
Call: “FBD/LD/IL View” menu
Requirements: The FBD/LD/IL editor is active.